Grove - High Temperature Sensor (SKU: 111020002)

Q1: Is the Temperature sensor analog or digital ?
A1: The High temperature sensor is an analog sensor.

Q2: Is there an example code for Raspberry Pi?
A2: The example library in wiki is for Arduino.

Please use the following resources to understand using GrovePi with sensors : Getting Started with GrovePi and GrovePi Software Examples

There are examples provided in the above links for Analog read using GrovePi. Modify them to use Grove - High Temperature Sensor.

反馈和知识库