Grove - I2C Color Sensor (SKU: SEN60256P)


  1. How to understand the commands? For example, REG_GREEN_LOW = 0xD0.

    From the attached picture, you can see what's in the command. When using byte protocol command, it must be like 0x80+ADDRESS. For example, REG_TIMING( 01h ) = 0x81
    For byte and block read, the command should be 0xC0+ADDRESS, REG_GREEN_LOW( 10h ) = 0xD0




Please visit our wiki page for more info about this product. It will be appreciated if you can help us improve the documents, add more demo code or tutorials. For technical support, please post your questions to our forum.




反馈和知识库