Wifi shield (Fi250) (SKU: 812001001)


1. How to use Wifi shield (Fi250) on Arduino UNO
  • ① Reset the module as factory default. Press the function three times at fast speed;
  • ② Upload sketch “Blink”(Arduino IDE: File - Examples - Basics) to Wifi Shield(Fi250); 
  • ③ Connect WIFI_TX to D1 and WIFI_RX to D0 with jumper hats on shield;
  • ④ Open Serial Port Tool, then send “AT+USET=baud rate,N,8,1,N”(Baud rate should be lower than 115200).
    For example, “AT+USET=38400,N,8,1,N”, and you will see “OK” returned.

    http://www.seeedstudio.com/wiki/images/b/be/Fi250_change_baudrate.jpg

  • ⑤ Change the jumper hats to connect WIFI_TX with D6 and WIFI_RX with D7.
  • ⑥ Upload the code below.
  • ⑦ Open serial monitor, and you will see it successfully joins wifi with the Red LED lit.

#include <Arduino.h>
#include <SoftwareSerial.h>
#include "WizFi250.h"
#define SSID      "Your-SSID"
#define KEY       "Password"
#define AUTH       "WPA2" 
#define spi_CS  8
SoftwareSerial uart(6, 7);
WizFi250 wizfi250(&uart);
void setup() {
Serial.begin(38400); //change to the right baud rate
uart.begin(38400); //change to the right baud rate
pinMode(spi_CS,OUTPUT);
digitalWrite(spi_CS,HIGH);
Serial.println("--------- WIZFI250 TEST --------");
// wait for initilization of Wizfi250
// wizfi250.reset();
  delay(1000);
  Serial.println("Join " SSID );
  delay(10);
  if (wizfi250.join(SSID, KEY, AUTH)) {
    Serial.println("Successfully join  "  SSID);
  } else {
     Serial.println("Failed join " SSID);
  }
  wizfi250.clear();
 Serial.println("*************send command to get Wizfi250 status******************");
  wizfi250.sendCommand("AT+WSTAT\r");
  //delay(10);
  char c;
  while (wizfi250.receive((uint8_t *)&c, 1, 100) > 0) {
    Serial.print((char)c);
  }
}
void loop() {
  while (wizfi250.available()) {
    Serial.write(wizfi250.read());
  }
  while (Serial.available()) {
    wizfi250.write(Serial.read());
}
}

Please visit our wiki page for more info about this product. It will be appreciated if you can help us improve the documents, add more demo code or tutorials. For technical support, please post your questions to our forum.


反馈和知识库