Xadow - NFC (SKU:WLS07111P)

  1. When the Xadow - NFC is connected to Xadow - mainboard, the connection between mainboard and the computer disappears.
    Please try to add the small battery to the Xadow Mainboard for more power while using Xadow NFC.
     2. Does Xadow – NFC have encryption?
Xadow NFC is based on PN532 chip. It supports MIFARE Classic 1K or MIFARE Classic 4K encryption in Reader/Writer mode.


Please visit our wiki page for more info about this product. It will be appreciated if you can help us improve the documents, add more demo code or tutorials. For technical support, please post your questions to our forum.




反馈和知识库