Xadow - Main Board (SKU:COM00100P)

  1. Dimensions (width, depth and height) of Xadow main board and each module.
  • Method One: Just Open It!
    Please download the Eagle file
    unzip it and open with Eagle
    you'll find the actual size of Xadow LOL.
    I have a screenshot which shows: 25.43 * 20.35 currently all Xadow module share the same size.
    http://www.seeedstudio.com/wiki/images/thumb/6/6f/Xadow-eagle-screenshot.jpg/800px-Xadow-eagle-screenshot.jpg
  • Method Two: Just Measure It!
    I get a sample size from my calliper, which show the size of Xadow Main Boad is: 25.96 * 20.27 * 2.58
    We have done 3D enclosure based on Xadow, We will write about design works on Xadow recently once I get free.
    PS: the height of Xadow modules are different due to different component are used, for example OLED is much higher~ I suggest you use a vernier calliper for precise size.
  2. I got this error while installing driver for Xadow Mainboard on Linux: usb device not recognized
  • As for a temporal solution, you can hold the reset button(Main board); and click the Upload button(Arduino IDE); release the reset button while the IDE monitor occur Uploading......


Please visit our wiki page for more info about this product. It will be appreciated if you can help us improve the documents, add more demo code or tutorials. For technical support, please post your questions to our forum.





反馈和知识库