Fusion PCBA Specification

Fusion PCBA Specification | |||||||||||||
Order Quantity | 1-8000pcs | ||||||||||||
PCB Layers | 1-16 layers | ||||||||||||
PCB Material | Rigid, Aluminum, Flexible Printed Circuit | ||||||||||||
Components | Seeed OPL | ||||||||||||
Components from Official Suppliers like Digikey, Mouser, Arrow, Element14 and others. They must satisfy the following criteria: 1). Must be allowed to be imported into Mainland China 2). Must be in stock or have a certain lead time 3). Must be available in small quantities or in the specified quantity. | |||||||||||||
Environmental standard | RoHS (Lead Free) | ||||||||||||
Solder Type | Manual Soldering/Surface Mounted Technology | ||||||||||||
Board dimensions | Minimum Size: 1.0mm*1.0mm | ||||||||||||
Maximum Size: 500mm*500mm | |||||||||||||
Board Shape | Various Shapes | ||||||||||||
PCB Design File Format | Gerber File | ||||||||||||
BOM (Bill of Materials) | 1. BOM file should be in csv, xls, xlsx format 2. BOM content should be as below
|
- PCBA Quick Answers
1 | We can assembly both sides (Components can be soldered on the top and bottom sides). |
2 | If possible, please provide us with a pick and place file (XY or Centroid file) in the PCB Gerber zip file. |
3 | Shipping is FREE to anywhere in the world for PCBA orders. |
4 | Stencils are included in PCBA orders but they are not shipped with the boards due to the high shipping costs. If you need stencils, please order them separately. |
5 | If possible, please keep all through-hole components on the same side (top or bottom). |
6 | The distance between 2 solder pads of 0402 components should be 0.26-0.45mm. |
7 | Please ensure that designator labels on the silkscreen are not on top of pads or vias since any overlapping silkscreen is removed during PCB manufacture. |
8 | Please clearly mark the pole for polarised components. |
9 | Minimum trace/vias/pads spacing is 4mil |
10 | The distance between any two chip components should be at least 1mm; the distance between chip components and connectors should be at least 5mm |
11 | Please maintain a clearance of 3.8mm around large ICs (48pins or more) and BGAs. The minimum BGA is 0.25mm |
12 | The solder pad size (length/width) on PCB should be larger than the pin size of the component |
13 | Temperature-sensitive components (e.g. LED, battery) may be damaged in the manual soldering process |
14 | The distance between soldering points and neighbouring SMD components should be at least 1mm |
- Gerber
- BOM File
2). SKU = "OPL P/N" = MPN
3). Parts = Designator = location (the location of your components)
3). If one SKU has a quantity of 3, please use this format: SKU: 318020010 Qty: 3 Parts: A4,C2,C3
Part/Designator | Manufacturer Part Number/Seeed SKU |
Quantity |
A4,C2,C3 | 318020010 | 3 |
C1,C2,C3,C4,C5 | RHA0J471MCN1GS | 5 |
D1 | ESP-WROOM-02 | 1 |
- Lead time:
The lead time for PCB Assembly orders is around 7-15 business days if all the parts are from the Seeed's OPL and around 20-25 business days if not. Please see below for details.
- PCB in production: PCB is being produced (3 - 14 business days, see note 1).
- BOM Processing: The procurement of components and other materials (around 18 business days from order confirmation).
- Assembly: The boards will be assembled and shipped 3 business days.
2. PCB production takes 3 - 14 business days depending on specific order parameters, not including delays caused by problems with the order/files, but typical boards are completed within 3 to 5 days.
3. We strongly advise customers to place orders well in advance of deadlines in case of any delays caused by problems with the order/files.
- Designator
The designators in uploaded BOM must comply with the ones in Gerber or in component placement file
- Package
The component package in the uploaded BOM should match the pads in the Gerber file.
- Polarity
Polarised components should have clear indications to their polarity on the silkscreen. Otherwise, the components may be incorrectly mounted.
- Quantity
Notice: Please examine the files carefully before placing an order. We are not able to change the Gerber files once PCB fabrication begins.