WiFi Shield (SKU: WLS06201P)

  1. Trouble shooting back to factory settings
  2.  Hardware factory reset 

  3.  
How to set a configuration when using WiFi shield with Mega?
  • Connect D2 to D10 then D3 to D11 by jumper wires           
  • Modify the program: Wifly(2,3); → Wifly(10,11);
More information about Software serial please refer to SoftwareSerial Library.

  4.  Will Wifi Shield be compatible with Arduino due?

  5. How to improve the connectivity between the Wifi Shield and the router?
      Do not place plastic or any other dielectric material in touch with the antenna. Any metallic objects in close proximity to the antenna will prevent the antenna from radiating freely.






Please visit our wiki page for more info about this product. It will be appreciated if you can help us improve the documents, add more demo code or tutorials. For technical support, please post your questions to our forum.

反馈和知识库