CAM/DRCデザインファイルダウンロード

 2019.10.28 から
FAQ内容の更新はFusionPCBブロクに移行いたします。
#全部済ませるまで引き続き元のFAQご利用くださいようによろしくお願いします。

Screen reader support enabled.
 


A few notes first, I recommend that you update to the latest Eagle version and use the built-in CAM files since they do resolve a few problems that were present in the past. I can't remember the details but generally it is better.

CAM ファイルダウンロード
2層 CAM ファイル 
4層 CAM ファイル   

Similarly, for the DRU files, they were taken down since they caused customers some confusion. For example, the minimum drill hole diameter is 0.3mm but actually you can have 0.2mm drill holes, they just cost extra. So, is that a DRU violation or not? It depends on the customer's budget.

DRU files (Eagle 向け) (最新のeagle バージョン で開けるのはお勧めです)

注意点:
1.カバーデータの全ては参考例なので、決してファイル通りに設計するではありません。初心者の方にはお勧めです。
2.ビア設定は一般的な設計に向けもので、DRCのままに設定する必要がありません。

ご参考まで



Feedback and Knowledge Base