Base Shield V2 (SKU: 103030000)

Q1: Does the Base shield work with 3.3V boards?
A1: Yes, When using Arduino UNO with Base Shield v2, please turn the switch to 5v position; While using Seeeduino Arch with Base Shield v2, please turn the switch to 3.3v.

Q2: Does the Base shield work with Seeeduino V3 boards? 
A2: Yes, please solder the pads, P1 and P2 if use Base Shield v2 with Seeeduino V3.

Q3: Where can I find technical support if I have some other issue.
A3: Please send an email to techsupport@seeed.cc

反馈和知识库