Seeed PCBA Functional Testing


Seeed Fusion offers Functional Testing (FCT) and other testing and programming services for PCB assembly orders. Performed after assembly and general inspections, functional testing is a surefire way of ensuring your boards coming off the production line work as intended. 

While Seeed will follow international assembly and quality control guidelines to maximize yield, as with any manufacturing process, there is always the potential for failures. Even more so with small batch or prototype assembly on a mixed line. As such, it is common to employ a functional testing program to isolate defective boards, whether the problem is incorrectly placed parts, failed joints or defective components - defects that may be difficult or impossible to catch with visual inspection alone.

Functional testing can be anything from a simple power-on test, point-to-point voltage testing, to running test firmware with custom-made jigs. Our lines are equipped with the essentials such as multimeters and function generators but Seeed also has the capability to develop test jigs and perform more advanced testing protocols. Please see the table below for more details. 

Seeed Fusion is now offering free functional testing with all PCBA orders. Verify the entire turnkey process and highlight defective batches with a quick test.

To add functional testing to your order, just select 100% Functional Testing in the PCBA section of the order page. Upload your test plan and test materials and add the order to the cart. 

For 100% testing, the system will automatically deduct the cost. You can also upload the test plan after adding your order to the cart, or any time before the boards are complete, but make sure to get them in early so we can prepare in advance. The total production time will be extended according to the total testing time required.

Example simple test plan:

1) Apply 9.9V to the contacts as shown.
2) One LED should light up.
3) Change the voltage to 12.6V and press the button once.
4) Five LEDs should light up.


Seeed Fusion PCBA Testing Capabilities


Category Product Function  Test Type Required File Test Location



MCU 
51 serial MCU IC Programming Firmware   Seeed's Fab
AVR serial MCU IC Programming Firmware   Seeed's Fab
ARM Cortex M0,M0+,M3,M4 serial IC Programming Firmware   Seeed's Fab





General Features
GPIO Functional Tes Functional Test Test Software   Seeed's Fab
Voltage/Electricity Current/ Resistance Test Functional Test Test Software Test Index Seeed's Fab
I2C/Uart/SPI/CAN/One wire/SWD Functional Test Test Software Test Index Seeed's Fab
Temperature/ Humidity/ Atmospheric Pressure/ Luminance Functional Test Test Software Test Index Seeed's Fab
More        











Communication
GSM/WCDMA/LTE Functional Test Test Software Test Index Seeed's Fab
GNSS Functional Test Test Software Test Index Seeed's Fab
Bluetooth/LE Functional Test Test Software Test Index Seeed's Fab
Ethernet Functional Test Test Software Test Index Seeed's Fab
NFC Functional Test Test Software Test Index Seeed's Fab
802.11/b/g/n/a/ac Functional Test Test Software Test Index Seeed's Fab
zigBee Functional Test Test Software Test Index Seeed's Fab
Sub-1 GHz 315/433/868/915 Functional Test Test Software Test Index Seeed's Fab
Monoboard Computer Beagle Bone/Raspberry pi/…… Functional Test Test Software Test Index Seeed's Fab
Certificate FCC/CE/GS/Telec/…… Regulatory Certification Test Software Test Index Lab

Please note, high precision testing and high voltage testing or any operations that pose a health risk to technicians will not be accepted. Customers will be expected to pay for any specialist tools or materials required for testing.


Last Modified 2024/01/19

反馈和知识库