My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
308 results found
-
Particle Asset Tracket
Paricle Asset Tracker
1 vote -
One twisted pair 100Mbit Ethernet
Hello guys. I would like to recomend to focus on Automotive ethernet, standard 100baseT1 (BroadR-Reach). Example of PHY nxp TJA1100,
It can be used in place original PHY of regular 100baseT Ethernet PHY. It is much more robust against EMI than PC version. It is already used in BMW. I can imagine nice, small kit that has on one side MII to interface MCU and on another IEEE802.3bw (3rd name for this ETH standard)1 vote -
Beaglebone Green Wireless+Ethernet
Industrial applications may require an ethernet and wifi connection at the same time. A beaglebone green wireless with ethernet port would be great. Does Seedstudio plan on such a device any time soon?
2 votes -
wrong link on RFbee page
check link on RFBee page: www.seeedstudio.com/wiki/index.php?title=RFbee_V1.1_-_Wireless_Arduino_compatible_node
I get "Page not found"
nils@meditalk.com1 vote -
Add a way to confirm receiving of parcel with order
I received my orders some days ago but its status still "Traceable"
4 votes -
Better Competitive Shipping
Affordable shipping options to Canada
1 vote -
3 votes
-
Offer Selective Laser Sintering (SLS) 3D printing services; if so when?
SLS is more effective for convoluted/complex shapes than FDM.
1 vote -
rechargable unit
mini solar panel, can charge on-board 9v battery
1 vote -
Exclude discontinued items from listings.
It's getting where there are more discontinued items than new ones. It would be nice if the discontinued items were only visible if you visited the item directly. (Preventing broken links). Otherwise exclude them from the default view.
3 votes -
Your mobile site stinks
Include the option to choose desktop site view on all devices.
3 votes -
LoRa GW, SKU 110060623, would sell well at $200
There are a number of "complete LoRaWan gateway" in the $240 to $300 range... Making this incomplete KIT expensive...
1 vote -
make it clear what order statuses are on web
on website under order keep status of the order updated like:
- validating order
- manufacturing started:
- stencil done (10%)
- routing done (30%)
- vias done (40%)
- solder mask done (70%)
- packing done (100%)
- shipped out2 votes -
Split shipping packages
Is any way possible to add an option to split the number of packages? I need 400 boards in 4 packages
1 vote -
UPS board for generic SBC
There are few boards with native lithium battery support but it would be nice to add UPS like function to any 5V powered board, be it ARM or Atmel. AXP209 is integrated on some boards and I believe it would be very interesting to have it on a breakout board similar with a solar charge controller. The simplest configuration would have only 6 pins (5V--In&GND / Batt+&Batt- / 5V-Out&GND). Some extra feature would make it even better: an EN pin that would cut-off both battery and Vin input. An AO pin to measure the battery voltage, a DO to send…
3 votes -
include the tubing for the smart plant care kit fir arduino. Or at the very least include the specifications for the vinyl tubing.
I had to order vinyl tubing because it was not included in the kit. There are no specifications for the tubing so I ordered something that looked like it would work. As it turns out the vinyl tubing that I ordered was incorrect so i had to order another size of vinyl tubing. After ordering 2 packages of vinyl tubing through Amazon and waiting over 2 weeks i finally got tubing that fit (on one part of the kit but not the other). I am very frustrated because this could be easily avoided with better instructions or the inclusion of…
1 vote -
A better support from SeeedStudio
Pretty simple a better support.
It is a must.
7 votes -
24-bit 192 kHz 120 dB S/N audio DAC
A reference quality 24-bit, 192 kHz, >120 dB S/N ratio audio DAC cape for all Beagle Bones.
1 vote -
that you PLEASE fix the wiki for GPRS Shield V2.0
that you PLEASE fix the wiki page for GPRS Shield V2.0.
It comes up totally blank.
http://wiki.seeedstudio.com/wiki/GPRS_Shield_V2.01 vote -
Add button to change order status in order history
In my order history I have several order marked as "Traceable" but I receive the order.
Add a user button to change the status to "Finisced"
1 vote
- Don't see your idea?