My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
-
new connectors needed
flat cable 2x40 pins low cost IDE specs
connector male IDE 2x40 specs, to construct flat cable connection
to mate with Mega edge connector
connector 2x8 female IDE connector for flat cablesmale connectors and male pins to construct Grove connector
RC plane (yes airplane) LI-PO battery connectors male females with male/females pins to construct longer cable connection
ONE to Many connector like 2- input female pins to insert to connector with connector other side has 8 output to insert male or female pins, called distribution connector, just like the black 0.1"(2.54mm) crimp connector.
this connector does not exists yet…1 vote -
2 votes
-
WebSite Bug Report: Cart Icon not updating
I had three PCBs loaded in the cart, yet the little icon (upper right corner) still showed '1', then added 4th PCB and shopping cart icon finally incremented to '3' -- but still not correct!
1 vote -
Hi people. Re Bus Pirate V4. Screw hole size change to suit case.
Hi people. Re Bus Pirate V4. The acrylic case kit has 3 mm screws, but the screw holes on PCB are only 2.8 mm after plating, and plating is used as part of ground connection, so drilling out is undesirable. Suggest you use 3.3 mm holes pre-plate on any rerun of boards.
3 votes -
Re-order
Re-order from old bazaar history
1 vote -
DHL account
We have DHL account already. Please give us an option to use our own DHL account.
3 votes -
Beaglebone Industrial
It would be nice to have an option where Industrial range components are used on the beaglebone green.
Quickly looking at the BOM, there are four components, all have -40 to +85C equivalents so a relatively simple change.2 votes -
Fix broken links to tutorials and drivers for ALL products. I'm shopping at adafruit till ya fix it !!! They have thier act together!!
Fix broken links to tutorials and drivers for ALL products. I'm shopping at adafruit till ya fix it !!! They have thier act together!
1 vote -
Get rid of Fusion PCB service
My experience with your fusion service has been appaling to say the least. I have ordered PCB fabrication and assembly from all over the world. Here in USA, where I am located, I get constant updates and can communicate with the PCB vendor. Just for your information, I have ordered from, Ireland, Romania , Canada to name a few. All of these places provide some communication on the process.
In Seeds case, not only was I unable to communicate with the PCB fab, but they issues a "shipped" notice and refused to answer my repeated emails on why I could…
7 votes -
New website homepage has no Login button
The homepage has no login or account info at all. I eventually found it on "Propagate" page.
9 votes -
Create a section in Spanish
My idea is that an area is created in Spanish, with all sections that exist in English, as there are currently 560 million Spanish speakers on the planet.
So, it would be a great success for the company.1 vote -
make a tool to update the rephone firmware from Linux or at least Windows 10.
I spent money and nothing works without a firmware update, I have Ubuntu and Windows 10 machines, advertised as open source, then tell me how to use any tool to update the firmware, it cannot be that complex, set in to firmware loading mode, transfer. bin file, disable firmware loading mode. or give me a couple of hundred dollars of credit for the money you took from me and lied to get, you have lots of great products and rephone should be one of the best but it isn't versatile enough to develop on. mac and Linux support will make…
3 votes -
PCBA with < 50 pieces/board cost much more than PCBA with > 50 pieces???? Why
I do calculation from your PCBA specification and I see board with < 50 pieces cost $0.10 per pin and board with > 50 pieces cost $0.01 per pin.
This pricing policy of yours means that a simple board cost more than a complex board.
This is a silly policy. We are looking for a manufacturer to produce thousands of boards for us, so I think we will use a different company because your cost is bad.3 votes -
Tough Stuff
Make it sturdy and tough. I barely placed the USB connection in and it broke.
Seth
1 vote -
"Processing" is not a very descriptive way of telling me where my project is at.
I can't see any deeper information than that my project is "processing" what does this mean? When can I expect it to change?
1 vote -
No pagination would be great, instead use "infinite" scroll
I really don't like browsing in paginated overview pages
3 votes -
Please add the 5 GHz to your BeagleBone Green! Or launch the BeagleBone Orange with the 5 GHz only WLAN. Should be rather easy to do...
Without doing my homework I think that the 5 GHz WLAN could be done just by WLAN controller and crystal changes and even the board could be essentially the same.
3 votes -
Create a http://www.seeedstudio.com/customer_service.html page that will not say code is not correct so people can contact you
I get a "{"success":"fales","msg":"You did not entered the validation code correctly. Please, try again."}" message after 10 tries with different codes on 2 different browsers.
Obvious you don't want to be contacted, convenient way to not have to deal with customer inquires.
1 vote -
add re order tap to PCB order history (ie as it was).
add re order tap to PCB order history (ie as it was).
2 votes -
I suggest you have a loot at this interesting open source bluetooth tag with sensors
Check this out https://github.com/ruuvi/ruuvitag_hw
They are launching a funding campaign, but all the stuff seems to be open source. I think there would be a lot of interest in tags like this. Would you consider manufacturing it?6 votes
- Don't see your idea?