How to export the correct drilling layer from eagle

Since we received many orders with no drilling layer or drilling layer error. So we analyze the reason and write this article. Hope it will help you.

Choose "EXCELLON" on the device drop-down box.And choose the layers  20(dimension), 44(drilles), 45(holes) .
(Sorry, may change to a English operating interface later.)  


To avoid this problem happen again, we suggest you download the newest CAM software from our website. We have already set the specification of CAM, then you can directly export the gerber file with correct Drill drawing layer.


If you still have problem to export the drilling layer, feel free to contact us.


Fusion technical support

  1. What is Gerber file?
  2. What are the PCB panelization rules?
  3. How to generate Gerber file
  4. How to export the drill files correctly?
  5. What is the correct way to draw the silkscreen on the bottom side?
  6. If my PCB does not require Solder Mask, what should I do?
  7. If my PCB do not require Drilling Holes, what should i do ?
  8. Which layer should I use in EAGLE for milling?
  9. What is the depth of the v- cut?
  10. If my PCB's do not have the silkscreen, how can I proceed with my PCBA order?
  11. Exporting manufacturing files from Altium Designer
  12. Export PCB gerber from Cam
  13. How to export the correct drilling layer from eagle
  14. What is the minimum trace width?
  15. What are the dimensions for Dielectric Separation thickness?
  16. What is the inner layer copper thickness?
  17. What is the range for the drilling hole diameter?
  18. What is Blind/Buried Via?
  19. What is the The Min Track/Spacing for 1oz./2oz./3oz. Copper weight
  20. How to output drill file correctly ?
  21. Is the board outline could only be rectangle ?
  22. What is the layer?
  23. What is Half-cut/Castellated Holes.
  24. How can i do if i do not required to make plated through holes?
  25. Options of Fiducial
  26. What is the size of the Fiducial?
  27. The dimension for PCB
  28. How do plated through slots work on the Gerber ?
  29. The material for FR-4/Aluminum Board/FPC
  30. The thickness of PCB
  31. The surface finish for PCB
  32. The color of solder mask
  33. The copper weight for PCB
  34. What is Impedance Control?
  35. PCB quantity
  36. How to generate Gerber files from PCBE
  37. How to generate Gerber file from Eagle
  38. How to generate Gerber files in Altium Designer
  39. How to generate Gerber file from KiCAD
  40. How to generate Gerber files in DipTrace
  41. How to generate Gerber files from Proteus
  42. How to generate Gerber files from DesignSpark
  43. Recommend size for BGA
  44. Solder Mask Dam
  45. Difference between standard PCB and Advanced PCB

Feedback and Knowledge Base