Exporting manufacturing files from Altium Designer

Kristoffer Stork wrote this article to help all the Altium users.  Thank you so much for his help.
To 
Kristoffer Stork:
  We sincerely appreciate your sharing!
                           Seeed
 
1. Setup Altium Designer to export RS-274-X formatted gerber files.
- Go to Tools - Preferences
- In the preferences options, open CAM editor and click on Import/Export
- Clicking the settings edits them

2. 
- Go to File - Fabrication Outputs - Gerber Files
- Read the quote furter down from seeedstudio on what files to export - this tells what to export.
- Use a mechanical layer as board outline. I use mechanical 1.


3. Now for the drill files.  
- Go to File - Fabrication Outputs - NC Drill files
- After hitting ok, you will be prompted to generate the files - simply click ok

4. Now, these files have been generated. (The ones under Generated - "Text documents" and "CAMtastic! documents")

- Right click on one file, select Explore - you should find all the generated files.

5. Zip all of these files, send them to manufacturing.

Especially this last part is a bit confusing if you are generating with Altium Designer. And yes, the .DRL gerber file that is generated with the NC drill generation do appear empty, but it is definitely needed.




Fusion technical support

  1. What is Gerber file?
  2. What are the PCB panelization rules?
  3. How to export the drill files correctly?
  4. Can I use another software beside Eagle to generate the Gerber files?
  5. What is the correct way to draw the silkscreen on the bottom side?
  6. If my PCB does not require Solder Mask, what should I do?
  7. If my PCB do not require Drilling Holes, what should i do ?
  8. Which layer should I use in EAGLE for milling?
  9. What is the depth of the v- cut?
  10. If my PCB's do not have the silkscreen, how can I proceed with my PCBA order?
  11. Exporting manufacturing files from Altium Designer
  12. Export PCB gerber from Cam
  13. How to generate gerber from KiCAD?
  14. How to export the correct drilling layer from eagle
  15. What is the Minimum inner trace width for 4 layers?
  16. What is the minimum trace width?
  17. What are the dimensions for Dielectric Separation thickness?
  18. What is the inner layer copper thickness?
  19. What is the range for the drilling hole diameter?
  20. How to Use Open Parts Library
  21. What is Blind/Buried Via?
  22. What is the The Min Track/Spacing for 1oz./2oz./3oz. Copper weight
  23. How to output drill file correctly ?
  24. Is the board outline could only be rectangle ?
  25. What is the layer?
  26. What is Half-cut/Castellated Holes.
  27. V-cut rules
  28. How can i do if i do not required to make plated through holes?
  29. Options of Fiducial
  30. What is the size of the Fiducial?
  31. How do plated through slots work on the Gerber ?
  32. The dimension for PCB
  33. The material for FR-4/Aluminum Board/FPC
  34. The thickness of PCB
  35. The surface finish for PCB
  36. The color of solder mask
  37. The copper weight for PCB
  38. What is Impedance Control?
  39. PCB quantity
  40. How to generate the gerber files from Altium Designer

Feedback and Knowledge Base