How to export the drill files correctly?

  • Please select EXCELLON instead of Gerber_RS274X when choosing the Device for Drill Data, this will help you eliminate the size problem.

  • If you use Altium, .TXT & .DRL are both acceptable.

  • Fusion technical support

    1. What is Gerber file?
    2. What are the PCB panelization rules?
    3. How to export the drill files correctly?
    4. Can I use another software beside Eagle to generate the Gerber files?
    5. What is the correct way to draw the silkscreen on the bottom side?
    6. If my PCB does not require Solder Mask, what should I do?
    7. If my PCB do not require Drilling Holes, what should i do ?
    8. Which layer should I use in EAGLE for milling?
    9. What is the depth of the v- cut?
    10. If my PCB's do not have the silkscreen, how can I proceed with my PCBA order?
    11. Exporting manufacturing files from Altium Designer
    12. Export PCB gerber from Cam
    13. How to generate gerber in KiCAD?
    14. How to export the correct drilling layer from eagle
    15. What is the Minimum inner trace width for 4 layers?
    16. What is the minimum trace width?
    17. What are the dimensions for Dielectric Separation thickness?
    18. What is the inner layer copper thickness?
    19. What is the range for the drilling hole diameter?
    20. What is Blind/Buried Via?
    21. What is the The Min Track/Spacing for 1oz./2oz./3oz. Copper weight
    22. How to output drill file correctly ?
    23. Is the board outline could only be rectangle ?
    24. What is the layer?
    25. What is Half-cut/Castellated Holes.
    26. V-cut rules
    27. How can i do if i do not required to make plated through holes?
    28. Options of Fiducial
    29. What is the size of the Fiducial?
    30. How do plated through slots work on the Gerber ?
    31. The dimension for PCB
    32. The material for FR-4/Aluminum Board/FPC
    33. The thickness of PCB
    34. The surface finish for PCB
    35. The color of solder mask
    36. The copper weight for PCB
    37. What is Impedance Control?
    38. PCB quantity
    39. How to generate the gerber files in Altium Designer
    40. How to generate Gerber files in DipTrace
    41. Recommend size for BGA
    42. Solder Mask Dam

    Feedback and Knowledge Base