The solution to your Roadrunner email problems!
If you are facing Roadrunner email problems then it is understood that you are unable to receive or send an email. There is nothing to worry about as we are here to provide you with a solution in both cases. If you are not receiving the emails then you should see if you have an active internet connection or not. If the network is not stable then you won’t be able to get an email. You should also see if the server is down or not by looking up the internet for the same. If you are not able to send an email then you should see if you have maxed out the limit or not as you can send 500 emails in a day.
https://www.emailtechnicalsupport.us/blog/roadrunner-email-problems/