Raspberry Pi support for Grove-TF Mini LiDAR
Raspberry Pi support for Grove-TF Mini LiDAR
-
robinmalhotra commented
Context: I tutor basic coding to people privately and semi-privately. Lately I've had more of the semi-privately (2 or 3 or 4 students at a time) classes, so I set up a projector in my officetel so that the students could all easily see my screen without craning their necks. Instead of hooking up a laptop or desktop to the projector, I found it more convenient to hook up an old Raspberry Pi with a wireless keyboard and mouse.
Specifically it's the original Raspberry Pi 1 B. For those who don't remember the old Raspberry Pi 1 Bs, the specs are:
Single-core 700MHz ARM (roughly comparable to a 300MHz Pentium II)
512MB RAM, shared with video (about 430MB available)
HDMI out
USB 2.0 and an SD reader
https://appsync.biz/abcya/ https://appsync.biz/adam4adam/ https://appsync.biz/pof/ -
Wittig Wendy commented
STD is no doubt a very known name and has affected millions of people out there. People living with STD are unable to find a correct life partner and are scared of coming out in the public. If you are also staying with the same then try STD dating sites. Hdatingsites.com is a perfect example for the same that offer dating opportunities to people with STD all for free. We also take the initiative to bring in correct knowledge and information. http://www.hdatingsites.com/