I suggest Seeed...

Example, Please on question "Which layer should I use in EAGLE for milling?"

On the answer for the question: "Which layer should I use in EAGLE for milling?", please include an example, like you do for the question about the Mask layer ("If my PCB does not require Solder Mask, what should I do?"). I.e. what kind of comment? is it "This layer is for milling"? or is there some other information needed. Also, are their any restrictions on milling? If that extra information is already available in another FAQ, then please include a reference (e.g. link).

BTW: Because there is no This Article Was Not Helpful" button, I clicked the "Flag this article as inaccurate" 'button' hoping it would open a dialog that would allow me to explain why. After clicking it, of course, I learned that this is NOT the case, but there is no Undo, so I couldn't un-click it!

BTW2: Thank you for all the FAQs (e.g. the Knowledge Base). They're awesome!!

1 vote
Vote
Sign in
(thinking…)
Sign in with: facebook google
Signed in as (Sign out)
You have left! (?) (thinking…)
Steve Lawson shared this idea  ·   ·  Flag idea as inappropriate…  ·  Admin →

0 comments

Sign in
(thinking…)
Sign in with: facebook google
Signed in as (Sign out)
Submitting...

Feedback and Knowledge Base