Raspberry Pi Case for WD Pi-Drive (or other 2.5" drive)
A choice of several cases is needed that can accommodate a RPi B/B+ board with a WD Pi-Drive (or similar 2.5" drives) that is compact and similar to most of the other cases that are available for the plain RPi boards. The modernistically-designed WD case just doesn't cut it. It is flimsy, difficult to access remaining USB connectors, and falls over too easily. The other WD case just sits on top of an existing case... again, not very convenient. A plain, simple enclosure is needed that allows for the RPi and Pi-Drive to be together in one case.

1 comment
-
Adminkavi (Admin, Seeedstudio) commented
We will surely consider your idea.A generic case including the driver would be a convenient option.