My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
308 results found
-
1 vote
-
Use PostNL as registered post for Europe instead of Singapore Post
to switch shipping provider and use PostNL. Other Chinese vendors offer it and it takes 10 working days to reach Europe at a comparative price.
Singapore Post is way too slow, and DHL/FedEX make sense only for large orders5 votes -
Use existing address information
Use the address you have on record for existing, logged in users. When I go to the checkout, I have to enter and address that you already have!
Lost sale there.1 vote -
Add 4x20 Grove LCD
The 2x16 Grove LCD is terrific, especially with the backlight color changes. Bring out a 4x20 version.
By the way, what are the hidden I2C addresses on this device? They should be documented so multiple devices can be used.
8 votes -
Please fix the shop category menu (and add a shopping cart/login button to the front page)!
The Shop category menu only works for me when I'm in the shopping cart page. It doesn't work (e.g. react to the mouse in any way) on any other page of the site (using Firefox, all plugins deactivated)!
Also, the white background of the sub-menus isn't optimal in my opinion as it doesn't contrast with the white page background.
And - why is there no cart/login button on the shop page!? The only way to get there seems to be to add an item to the cart.
This is another point: I iked the old behaviour more where you were…
1 vote -
Your Verification button says its case sensitive but codes only show upper case. In short it dont work!
Fix your Verification box so that it shows both upper and lower case letters properly. I do not have time to be dicking around trying to figgure this out.
3 votes -
Need to improve your suppy chain
My recent order experience...
Order Number: 204016 (item in stock)
Me: 03/23/2016 - Order placed
Seeedstudio: 03/23/2016 - Order comfirmed
Seeedstudio: 03/24/2016 - Traceable; "Shipped" per your CS
DHL: 03/24/2016 - Shipment information received
DHL: 03/30/2016 - Shipment picked up
DHL: 03/31/2016 - Shipment deliveredOrder Number: 204015 (PCB)
Me: 03/23/2016 - Order placed
Seeedstudio: 03/23/2016 - Order comfirmed
Seeedstudio: 03/29/2016 - "Shipped" per your CS
Seeedstudio: 03/30/2016 - Traceable
DHL: 03/30/2016 - Tracking number not found
DHL: 03/31/2016 - Shipment information received
DHL: 04/01/2016 - No update yet...When I contacted your Customer Service on 03/29/2016, they seemed to…
1 vote -
Add Mesh Support to Smart 7688 Duo
The ability to be both a Wifi station and a Wifi access point, simultaneously, would allow the Smart 7688 Duo to participate in powerful Mesh Networks. This can be accomplished virtually within a single radio (allowing for the same channel, or a more power-draining second radio). The 'hostapd' package in openwrt's Chaos Calmer supports this feature.
4 votes -
Sell the matching motor separately for the Tessel Servo Module
I just ordered Tessel Servo Module 108990016
It supports multiple motors but you only sell one of this specific motor with this item. You should also sell it individually. I had to go order it from another website so that I could have 2 of the same model motors.
In fact, it would be a good upsell link like "Customers buying this also purchased..."1 vote -
Email to Track and Trace number as soons as it comes available
Why I get an email to my order is traceable, but first I have to log in and go to the order history and there find the number.
Why not send the track and trace number in the email?4 votes -
Offer the 2-pin JST to JST SM cable from the EL Driver as a separate component
The Grove EL Driver comes with two cables. One of these is 2-pin JST to 2-pin JST SM for making the connection from the board to the EL Wire. My suggestion is to offer that cable as a separate item in quantities similar to those offered for Grove adapter cables.
1 vote -
Ethernet transceiver a bit noisy (but BBG is quiet in general!)
Make the ethernet transceiver radiate less. I did radiated emissions testing on the BeagleBone Green and it does quite well. It passes Class B residential, which is difficult to do. However, I had to add a ferrite on the ethernet cable. Your ethernet chip must be noisy. Thanks!
1 vote -
ZIP-Support
maybe you consider zip instead of rar?
All Windows users hav ZIP support by default but not rar.2 votes -
Your web pages are difficult to follow! Difficult to determine how to get special deals, and promotions.
Make it easier to order pc boards, include discount promotions, and checking on orders purchased! You have a great company, make it easier for the USA to place orders with you. Free shipping on pcb orders would greatly increase your business!
Stephen1 vote -
1 vote
-
drill dia.
upto 7.5mm drill diameter in fusion pcb
4 votes -
Human check / review option.
For new, first time users, add an option for a human review / check of the order on the phone with the customer. I'd pay extra for that.
4 votes -
to have a filter on 'discontinued' products and not show them in the search bar by default
to have a filter on 'discontinued' products and not show them in the search bar by default
11 votes -
BB green in a USB stick compact version - cost reduction could allow volume use for end user consumer products
BB green in a USB stick compact version - cost reduction could allow volume use for end user consumer products. What could be the cost in 10,000 volume?
4 votes -
webpage inprovements
Make sure your website works with tracking instead of allways saying processing
1 vote
- Don't see your idea?