My Seeed Idea
Share. Vote. Discuss. See.
Share your ideas, tell us what you think of other people’s ideas and join the discussion.
Idea Guidelines:
1 – Idea needs to be something we can do. This means, although we appreciate general feedback (for example, “this is good!” or “this hurts!”), here we are looking for ideas we can work on.
2 – Specific. The more details you can provide, the better. Heck—you can attach files to ideas or a reference link to show us what you want!
To get help or support, download, or more information, please visit our wiki site.
-
Liquid density and temperature sensor (sterilizable)
An addressable, 1 or 2-wire protocol reporting sensor that, when placed in a liquid could report on the temperature and density of that liquid.
This sensor could be used to determine specific gravity during brewing etc.
Also, as a secondary wish - adding a pH sensor would be awesome.
3 votes -
http://www.robotshop.com/en/300k-pixel-usb-20-mini-webcam.html
Hi, to write the driver of this camera http://www.robotshop.com/en/300k-pixel-usb-20-mini-webcam.html, i need its datasheet (its interrupts and how it works) where can i find it ?
Thank you in advance.
3 votes -
No pagination would be great, instead use "infinite" scroll
I really don't like browsing in paginated overview pages
3 votes -
Online health portal
I wish to have site like this https://peryourhealth.website which allows users to pay helthcare bills online. I wish to have download and update bill functionality as well
3 votes -
3 votes
-
Data storage expansion for the RePhone.
It would be great to be able to expand the RePhone memory, either to have a module that increases the flash memory or a module for a SD card reader, anything that could increase the only 5mb storage that is available in the RePhone.
3 votes -
BEST APP TO PLAY THE GAMES...
The best phase of all our life is Childhood...All the sweet memories are started there,like playing games...What ever you have played mostly the childhood games are included in this app...Like super mario etc.,Download the latest happy chick app for free...click here to download http://happychickapp.com
3 votes -
Correct your weeb page
http://www.seeedstudio.com/service/index.php?r=pcb&ref=bannerfusionfusion201631
in this page it says 4.9$ for 10 pcs but when you click it it changes to $9.9
why it is different ?3 votes -
Wireless charging for Super Capacitor
A wireless charger that can charge a Super Capacitor [SC]. It would have an adjustable maximum voltage of 2.0 to 2.5 volts, and be able to dump large amounts of current [5A or more -- much more] into an extremely low impedance load [i.e. a current source with an upper voltage limit]. Also, it should be able to dump current into the SC at full bore all the way up to the maximum voltage. A typical SC has a maximum voltage of 2.7 volts, but should not be charged higher than around 2.2 to 2.5 volts [the higher the voltage…
3 votes -
change settings of an order
on order nummer 170406231014 can i change the dimension in 100mm?*70mm?
and Layer into 1 and PCB color in blue ?
I have doing to wrong by doing first the setting and then upload the file.regards ronald
3 votes -
Test Your Webpage
For years everything worked seamlessly but now the webpage is full of bugs. Next to the user icon it shows "Hi,?????". Trying to order a Fusion PCB with Firefox everything works, except the "Add to Cart" button does nothing, I tried with 2 versions of FF. With Chromium the menu doesn't work, nothing happens if I move the mouse pointer to the "Fusion" menu. Pressing the mouse button opens the menu, but releasing it goes to a different page. Some links give a 504 error. My address book is empty and all old orders are gone too.
Please install a…3 votes -
Support nicknames for accounts in the Fusion gallery
At the moment the Fusion Gallery shows my real name. I'd prefer to use an alias, a nickname. Allowing nicknames would encourage me to share more projects.
3 votes -
3G support for Linkit One/Linkit A-Core
3G support for Linkit One
3 votes -
Cash App Phone Number- Always ready to Support on Square
Cash App is digital payment app owned by the Square Inc. as the parent company. Cash App allows users to both transfer and receive money online. For utilizing this app it is required to create an account using a mobile number or email ID. After logging into Cash App account one can easily send or receive money. Cash App has so many great features such as free cash card, direct deposit, cash app boost, and get free money on Cash App. The direct deposit on Cash App allows users to get the paychecks directly in the bank account.
cash app…3 votes -
Accurate shipping price evaluation (include import taxes for UPS/DHL/...)
I bought 10 PCB for 4€38 - 1€32 discount. (round to 4$).
I payed 21€38 shippement (round to 25$) using UPS.
So far so good, this was calculated and announced.
BUT I had to pay additional 20€ to UPS (round to 25$) (about 5€ VAT + 15€ fees for UPS ! )This fees are precisely calculated and could be known in advance, please include them (even just estimation) in cart page.
Simple first step could be to put a simple warning.PS: I do not even know how seeed earn money with such low prices
3 votes -
oximus smart watch manufacure
http://www.oximustechnologies.com @ Please do not worry - I'm helping you here. Otherwise it will be a shit post! I will show you how I became "smart • spender", but I am not a professional. I always my technique, self-confidence, as well as a little bit of "boring", we are working to find a system to get more for my money. So, what I explain to you is by no means a last resort. You should take it and adapt it to it using it. These are the tools I have given you. http://www.oximustechnologies.com/smart-watches.html
3 votes -
Get it Right the First Time
Board was not "V-Cut" as specified putting me behind schedule!
2 votes -
The grove serial mp3's sound is vastly superior than the grove mp3 v2.0 especially where volume control is concerned
I wish that either you do not retire the grove serial mp3 or try an other mp3 chip for a grove mp3 v3.0. thanks
2 votes -
当我选择国家为中国(China)时省份只能从下拉列表中选取中文省份,无法输入英文?地址又只能使用英文
当我选择国家为中国(China)时省份只能从下拉列表中选取中文省份,无法输入英文?地址又只能使用英文?
2 votes -
No registration is posible, pease analize why I can not register.
No register is possible. System Registration is working bad.
2 votes
- Don't see your idea?